Author Topic: Best USB stick for use with DP6xxLX  (Read 9416 times)

Offline BRIan

  • PLUS+1 Expert
  • ****
  • Posts: 60
  • Karma: +3/-0
Best USB stick for use with DP6xxLX
« on: November 20, 2013, 11:20:06 PM »
Some USB sticks are slower than others when used to download application logging from the displays. Has anybody got a brand/model number where they have had good experience?

Jerzy Smyl

  • Guest
Re: Best USB stick for use with DP6xxLX
« Reply #1 on: November 24, 2013, 10:42:14 PM »
Hi,

Over last few months I had chance to "play" with DP6xxLX and DP7xx and to be honest there is no much difference between different types/makes of memory sticks.If there is some I think that we cant even notice it.

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 352
  • Karma: +8/-0
    • Marbek Elektronik
Re: Best USB stick for use with DP6xxLX
« Reply #2 on: July 17, 2014, 10:51:45 AM »
HI,
does anyone knows, if DP6xxLX will be replaced by a new display ?
We need a low priced display which can support USB-Stick.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline jashom1

  • PLUS+1 Expert
  • ****
  • Posts: 80
  • Karma: +6/-0
Re: Best USB stick for use with DP6xxLX
« Reply #3 on: November 06, 2014, 11:36:34 PM »
I have just discovered that a Sandisk USB 3 memory stick does play havock with the display, the .csv file gets corrupted with random filenames etc that are exisiting on the USB drive.  The drive is an Ultrafit 64GB SDCZ43.  Not sure if this issue is just with this USB stick, or USB 3.0 devices in general.

Cheers,

John.