Author Topic: CAN Protocols  (Read 6277 times)

CPP

  • Guest
CAN Protocols
« on: April 12, 2013, 08:51:30 PM »
Is it possible to use multiple protocols on one 50pin controller?

ie. CAN_0 - J1939
     CAN_1 - CANOpen

Offline Lammert

  • PLUS+1 Developer
  • ***
  • Posts: 11
  • Karma: +0/-0
    • Hydro-CAN Engineering
Re: CAN Protocols
« Reply #1 on: April 12, 2013, 11:02:57 PM »
Hello,

There is no problem to do that. The both CAN clamps are separate from each other. Only be carefully that you don't use signals from J1939 to CAN_0 and then inside to CAN_1 and then to CANOpen. I had some trouble with.

Regards

Lammert