Author Topic: WS CAN 2  (Read 3310 times)

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
WS CAN 2
« on: August 14, 2020, 06:25:33 PM »
Hello Guys,

Does any one knows if there is a way to tell the Service Tool to use the CAN 2 of the WS503 instead of the CAN 1?

Basically when I do a remote connection with the service tool it uses the RP1210B gateway, and gets connected to the WS503, then I can see the devices on CAN 1 of the WS but the ones on CAN2.

thanks  for the advise

Regards

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
Re: WS CAN 2
« Reply #1 on: August 17, 2020, 03:38:42 PM »
for the record,

I had a reply from the Plus1 help and the answer is no, there is not way to switch to CAN 2 of the WS for flashing devices remotely.

Thanks