PLUS+1 User Forum
PLUS+1 Software => Displays => Topic started by: bgtwuk on November 14, 2010, 02:29:14 PM
-
Good Morning
I am new at this of course. I have two screen area pages, and am trying to select between them with a soft button.
I have an enable port for each page, that I believe should have the proper affect.
Am using a simple switch but my pages are not toggling properly.
The fog is thick up here eh!
Bgtwuk
-
Hi!
Have you connected your enabling signal inside the Area? It is very easy to forget.
(http://www.sauer-danfoss-plus1.com/Themes/Sauerdanfoss/images/Forum_Replies/Enable_Area_1.png)
(http://www.sauer-danfoss-plus1.com/Themes/Sauerdanfoss/images/Forum_Replies/Enable_Area_1_1.png)
Best regards // Thomas
-
Very Interesting.
I will try that.
Thanx
-
Hi,
I have another question about toggling area pages:
I have a program with very much area pages.
Now, I have to add a new area page which can be placed everytime and everywhere on display.
It is a "help-screen".
My question:
Is it OK to switch on this new area page and it will appear in front of all other areas?
If I switch off this help-menue it will disappear and the screen is as it was before this action.
Is there a rule like: The last area wins?
-
Hi Bernd
Yes that is correct.
And the last area of the enabled areas wins.
Best regards
Daniel
PLUS+1® HelpDesk
-
Thanks,
but one question about Thomas' two linked area pages from NOv. 15 2010:
Does it work if they are linked?
If I copy an area page and don't delete the linking of them, the compiler produces an error.
Is it possible to copy area pages and link them?
I think, there would be a problem, if you want to assign a screen page to one of them, because they have the same name.....
I'm working now with Guide 5.0.8 .