Author Topic: DM1000 button mapping  (Read 3105 times)

Offline drphil69

  • PLUS+1 Novice
  • *
  • Posts: 4
  • Karma: +0/-0
DM1000 button mapping
« on: January 09, 2023, 06:10:23 PM »
I started my first DM1000 project, and I am looking for the button mapping.  All the buttons are numbered, so I need a map to see what buttons correspond to the NAV buttons. 

Using hardware v. 2.45.  In the Buttons input page it states:  "TODO: image with button layout"

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 275
  • Karma: +26/-1
Re: DM1000 button mapping
« Reply #1 on: January 10, 2023, 07:08:45 AM »
Hello,

I believe you need to update your HWD file. The latest version in the PLUS+1 Update Center is 3.11.  (See forum topic: https://www.plus1forum.danfoss.com/index.php?topic=1624.0)
In this version you got a button layout in the input page (see image).

You can open the template in the Module Viewer from the hardware tab in GUIDE by right clicking the template (see Image). No need to install it to the project.


Good Luck
Best regards,
Tor
PLUS+1® SW PAE Team