PLUS+1 Software > Communication
Difference Between CAN 0 and CAN 1
(1/1)
jgarzon:
Hello My Friends
Something I'm new at this and I have a question
What Is the Difference Between CAN 0 and CAN 1?
Thanks in advance for the clarification of my question
_________________________________________________-
Hola Mis Amigos
Soy Algo Nuevo En Esto Y Tengo Una Pregunta
¿Cual Es La Diferencia Entre El CAN 0 y CAN 1?
Gracias De Antemano Por La Aclaracion De Mi Pregunta
hproffitt:
The main difference that I am aware of is that you can only download a new .lhx file to CAN0. Besides that, they are just two separate CAN channels that you are able to utilize to lower your bus load and/or separate functions that may interacting with a different location on the machine.
Navigation
[0] Message Index
Go to full version