PLUS+1 Hardware > Displays

PIB - DM1x00 HWD file update

(1/1)

Tor:
Hello,

If you have not seen the latest PIB (Product Information Bulletin) about the DM1x00 I would like to share it here.

In short:
An issue was found that can cause the device to lock and become unrecoverable. The advice is to recompile to .HWD v308 or greater for any devices with a manufacturing date of August 11 or after.
The HWDs are located in the PLUS+1 Update Center. The version stated in the Update Center is 3.8.0 for some reason, but it's v308 when installed in GUIDE.

More information in the attached image/PDF file.


Thank you.

Navigation

[0] Message Index

Go to full version