PLUS+1 Software > Communication
TTL Serial Communication
(1/1)
SunnyMan:
Hello,
we would like to convert the TTL serial signal of distance (ultrasonic sensor) to a MC012 Controller. Do anyone know or do anyone has experience how we can do it?
We can use a converter TTL/CAN, but I will try to connect it directly as our first step... if it possible, of sure :)
Thanks for any idea how to do it.
PS. The description of data of TTL protocol is attached.
Best regards
Michael
Marbek_Elektronik:
Only Controller with RS232 are Displays DP6xx and DP7xx and ....
MC012 can't do RS232.
What is the distance between sensor and Controller?
RS232 with 9600bit/s is to fast to handle without RS232-interface in controller.
If you wand to handle this manually, the bit-rate should be very slow.
I think, the best way is, to convert it to can-signal.
Navigation
[0] Message Index
Go to full version