PLUS+1 Tools > PLUS+1 GUIDE
Curved Monitor usefull ?
(1/1)
Marbek_Elektronik:
Hi,
I have a HP 30" Monitor.
I am thinking about curved monitor as computer players use.
Does anyone use such a monitor?
I think, the plane one is better than a curved one.
Lukey:
Cured monitors I think they are overrated/a gimmick, personally I use 3x 27".
Great for multi tasking, for example viewing, Guide, service tool and a data sheet
Tor:
Hello,
Can we keep this as a discussion if curved monitors are useful when developing in PLUS+1 GUIDE I will keep it here. In other cases I will move it to the "Off Topic" section.
For GUIDE developing I believe it can be a good thing. Large drawing on the screen, and everything at the same distance to your eyes. Your eyes don't have to re-focus as much when you are turning your head? This is what I think, I don't have any facts to back me up.
The curved monitor has become a standard in our office, but myself are using two 27" flat monitors and a laptop screen. I thought it got a little crowded running both Service Tool and GUIDE on the same monitor. And if I wanted the same setup as I have now, I would have to get a 49" curved monitor (If I remember correct) and that was not an option.
Have a nice Holiday.
Navigation
[0] Message Index
Go to full version