Author Topic: USB Storage Device not recognized when using CG150-2 and Service Tool ?  (Read 5572 times)

Offline Lukey

  • PLUS+1 Expert
  • ****
  • Posts: 67
  • Karma: +6/-0
USB Storage Device not recognized when using CG150-2 and Service Tool ?

Hardware is DM1x00 Displays, I have tried on both a DM1200T and DM1000T with no success.

Has anyone encountered this?

I am NOT able read/write/see my USB Storage Device connected to the M12, C4—USB Host port when using a CG150-2 and Service Tool

I am able read/write/see my USB Storage Device when using the USB Interlink and Service Tool which is connected on the M12, C3—USB Device port