Author Topic: POU Outputs as Image Signals  (Read 2509 times)

Offline THLL

  • PLUS+1 User
  • **
  • Posts: 8
  • Karma: +0/-0
POU Outputs as Image Signals
« on: December 20, 2019, 07:26:10 PM »
I am calling a POU output signal to drive an images rotation. However it never works on the display. I know the signal is good and working because it will work when I retype that signal then add it to the screens inputs without calling the POU, which defeats the purpose of calling the POU in the screen editor..

It is possible to have a POU output drive anything in screen editor?

Edit: Literally following the same steps as the tutorial https://www.youtube.com/watch?v=6E_9Hv-2Acc&t=432s
System: Display DP710 / Plus+1 v12.0
 
« Last Edit: December 20, 2019, 07:52:59 PM by THLL »

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +13/-0
Re: POU Outputs as Image Signals
« Reply #1 on: January 14, 2020, 02:03:02 PM »
Hello there THLL!

This should work. Maybe you could send us your application for us to take a look at it? Please send it in a .p1p-format, including any special fonts you've used, to plus1helpdesk@danfoss.com .

Best regards
Nilla
PLUS+1 Helpdesk team