Author Topic: BUS Load - CANOpen vs J1939  (Read 710 times)

Offline Lukey

  • PLUS+1 Developer
  • ***
  • Posts: 49
  • Karma: +5/-0
BUS Load - CANOpen vs J1939
« on: May 04, 2024, 02:18:11 AM »
Typically which protocol generates more bus load? Within a system of lots of nodes?

Often when selecting hardware like JS1H joysticks, PVE CAN coils and other Danfoss sensor there is always both options CANOpen Or J1939.

Almost all my applications are using a GUIDE controller so there is no limitations there, I'm not concerned about the pros or cons of each protocol but concerned when designing a system with lots of nodes/devices, which would be best to select to reduce bus load?