Author Topic: Multiple MC Modules?  (Read 4485 times)

CPP

  • Guest
Multiple MC Modules?
« on: February 10, 2014, 07:07:32 PM »
Due to space and I?O requirements I am needing to use two MC050-010 modules and some OX modules in the same system. Is there a way to do this or are the two MC's just going to conflict with each other?

Offline BRIan

  • PLUS+1 Expert
  • ****
  • Posts: 56
  • Karma: +3/-0
Re: Multiple MC Modules?
« Reply #1 on: February 10, 2014, 10:39:04 PM »
This is one major selling point of the PLUS+1 ie expandable.
You just need to give each module a unique ID.

Offline spittet

  • PLUS+1 Guru
  • *****
  • Posts: 117
  • Karma: +6/-1
Re: Multiple MC Modules?
« Reply #2 on: February 11, 2014, 03:52:39 PM »
Also, you may want to keep one MC050 as a "custom" IO unit. I mean, use a MC050 without any bulk/programmable content in it. Only use CAN messages that are directly connected to inputs and outputs of this MC050.

My point is to do not have half a program into a MC050 and the other half into the other MC050 for the sake of easy maintenance and upgrading in the future.

Sam