PLUS+ Tools > PLUS+1 and C

Structured Text POUs vs. CCPs

(1/1)

FluidPowerTom:
I haven't yet used GUIDE (training next month), so I don't know the extent of the seemingly new structured text POU functionality.  Does it largely replace the need for injecting in custom C/C++ libraries via CCPs?

Thanks,

Tom

Daniel:
Hi Tom,

Yes and no; while there is some overlap between the two features, their main purposes are different:

* The main purpose of being able to import C libraries via CCPs is to be able to reuse legacy C code.
* The main purpose of being able to write Structured Text code in GUIDE is to allow use of industry standard code for PLC programming.Currently, if there is a need for text based code in GUIDE, then Structured Text is the preferred and easiest method to use.

Best regards
Daniel
PLUS+1® HelpDesk

Navigation

[0] Message Index

Go to full version