Author Topic: How to play a recorded file?  (Read 11699 times)

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
How to play a recorded file?
« on: February 20, 2015, 09:53:08 AM »
Hi,
I have logged CAN data to a text file.
But how to play this file back to can bus?
Can anybody help?
Thanks,
Bernd
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: How to play a recorded file?
« Reply #1 on: February 20, 2015, 10:40:27 AM »
I have found it in "View HistoryList/ Load *.txt"
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Jakob

  • PLUS+1 Expert
  • ****
  • Posts: 98
  • Karma: +2/-0
Re: How to play a recorded file?
« Reply #2 on: February 20, 2015, 11:03:09 AM »
Nice :)
I was wondering if the historylist function could do this.

Offline hgb1992

  • PLUS+1 Developer
  • ***
  • Posts: 13
  • Karma: +0/-0
Re: How to play a recorded file?
« Reply #3 on: March 11, 2015, 11:59:32 AM »
Hello!

Did the function "view history list/load" solve your Problem? Such a function would be very interessting for me too!

Thanks in advance for your Feedback.

KR, Benedikt

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: How to play a recorded file?
« Reply #4 on: March 11, 2015, 03:40:59 PM »
it is very tricky to use:

At the time, it works only if I use the Kvaser CANKing (installed Danfoss CANKing parallel, because of drivers),
and in second: work with Dez-formatters, not with Hex-formatters!
In Window "Select Formatters" click on "options" and select "Dezimal"

Perhaps it works better, if you use original Kvaser software and an Kvaser gateway?
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline SunnyMan

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
Re: How to play a recorded file?
« Reply #5 on: December 02, 2015, 04:28:20 PM »
Hi to all,

I found a X-Analyzer3 software few days ago... I am satisfied of features of this soft so much, even it can to playback a log.

Now the ECO version of this soft is free of charge, just to buy one Kvaser Leaf Light 2.0 interface.

http://www.xanalyser.com/xanalyser3/videos/

MJ