PLUS+1 Software > General controls
How to save a STRING to NV?
spittet:
--- Quote from: FluidPowerTom on September 02, 2020, 06:09:30 PM ---I'd be checking to see if STRING type variables will save as RETAIN variables in the Structured Text POU. That'd be by far the easiest way.
--- End quote ---
I tried it and, unfortunately, it seems that a variable of String type cannot be set as "RETAIN" in ST. I got the following message in the "Compiler Messages" during compilation (that aborted) :
--- Code: ---st_SavedString_data has a non-basic type, and can therefore not be backed by Non-Volatile memory
--- End code ---
I joined the test project to this post
acmall:
See this post from Nilla about limited support for RETAIN: -
https://www.plus1forum.danfoss.com/index.php?topic=1157.msg3763#msg3763
Sergio-DEK:
I agree. Expanding the support for NV and RETAIN variables is long overdue.
macbahi:
Hi All,
I downloaded the program SaveStringNV and I modified.
It's working but the data it's not saved as in NV.
when the controller is off, the SaveString data it's not saved .
Please are you finding a why to save string?
I need that to integrate a password in our program for customers.
Thanks in advance for your help
With best regards
FluidPowerTom:
It sounds like the only way to do it with Danfoss hardware may be to set up an ASCII lookup table and actually save the values as number arrays.
Navigation
[0] Message Index
[*] Previous page
Go to full version