Author Topic: Fault Manager Library  (Read 6468 times)

Offline deaks57

  • PLUS+1 Developer
  • ***
  • Posts: 24
  • Karma: +3/-0
Fault Manager Library
« on: February 21, 2020, 01:56:22 AM »
Has anyone used this yet?
Is it possible to use this to convert SPN/FMI from an engine and display text equivalent?
Cheers

Offline FStelzer

  • PLUS+1 Expert
  • ****
  • Posts: 50
  • Karma: +8/-0
Re: Fault Manager Library
« Reply #1 on: March 02, 2020, 08:12:16 AM »
Hi,

theoretically it's possible with a lot of work in coding ;) The amount of possible errors to store in the fault manager is also limited - so it will be not possible to catch all SPN/FMI faults from an engine.

For me, the fault manager is used to generate your own SPN/FMI codes out of the errors in your application. You can also create standardized DM1/DM2 messages with the SPN/FMI codes.

Regards,
FStelzer

Offline dlewis

  • PLUS+1 Guru
  • *****
  • Posts: 103
  • Karma: +2/-0
    • Getman Corporation
Re: Fault Manager Library
« Reply #2 on: January 25, 2021, 02:40:53 PM »
I would love to use this feature if it does what I think it does, but when I try to build the spreadsheet it tells me "Bad file name or number".  Not sure what that is all about.