Author Topic: Can not open pdf files in Guide  (Read 5123 times)

bgtwuk

  • Guest
Can not open pdf files in Guide
« on: December 23, 2014, 02:14:12 AM »
Hi Gents

I can not seem to open any of the pdf's within guide.

It just ignors the request.

Help

Bgtwuk

Offline oiltronic

  • PLUS+1 Guru
  • *****
  • Posts: 170
  • Karma: +15/-0
Re: Can not open pdf files in Guide
« Reply #1 on: December 24, 2014, 11:27:02 PM »
Can you open them from the Windows file manager with a double click or do you need to pick the application first?  If so, and using Windows 7, go to a PDF file in File Manager, right-click on the file, select "Open with" then "Choose default program...". 

Offline CShultz

  • PLUS+1 Developer
  • ***
  • Posts: 25
  • Karma: +0/-0
    • TST Hydraulics
Re: Can not open pdf files in Guide
« Reply #2 on: December 27, 2014, 04:37:05 AM »
I've experienced a similar issue.  If I have a PDF open from GUIDE I cannot open PDFs from my PC and vice versa (I think if my memory is correct).  I am sure its an adobe setting I may need to change but the issue was not that important to me. 

bgtwuk

  • Guest
Re: Can not open pdf files in Guide
« Reply #3 on: December 30, 2014, 10:09:14 PM »
can open them if I save it to another location.

But cannot open them while in Guide.

Bgtwuk

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 352
  • Karma: +8/-0
    • Marbek Elektronik
Re: Can not open pdf files in Guide
« Reply #4 on: June 10, 2015, 01:09:35 PM »
If I have opened a  PDF-file in Guide,
I use another PDF-reader, like Nitro Pro 8 test version, to open other pdf-files,
because Acrobat Reader doesn't work in parallel with Guide.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung