Author Topic: display fails  (Read 5541 times)

campodavila

  • Guest
display fails
« on: January 13, 2014, 03:02:27 PM »
Hello
How can I know if de display DP620 has internal fails
from another sauer controller

thanks

Offline oiltronic

  • PLUS+1 Guru
  • *****
  • Posts: 170
  • Karma: +15/-0
Re: display fails
« Reply #1 on: January 25, 2014, 02:11:53 AM »
One way is to send a custom CAN message from the screen to the other controller, and put status flags or an error code number in the message.

Cristian

  • Guest
Re: display fails
« Reply #2 on: March 20, 2014, 02:28:28 PM »
Hello Campodavila,

can you please explain better your issue?

Do you maybe mean your display get stuck beacuse a controller connected to it?

If the answer is yes, I got the same problem and not yet figure out how is possible...

Let me know

Cristian

Offline oiltronic

  • PLUS+1 Guru
  • *****
  • Posts: 170
  • Karma: +15/-0
Re: display fails
« Reply #3 on: April 05, 2014, 08:30:26 PM »
display get stuck beacuse a controller connected to it

Can you explain this a bit more?  Do you mean that a display appeared to freeze, crash, ignore CAN messages, or something else?  And what do you mean by "connect"?  Electrically added to the same CAN bus, sending any CAN message, etc?