Author Topic: PVE-P  (Read 4982 times)

Brant

  • Guest
PVE-P
« on: October 18, 2012, 08:57:43 AM »
Hi everybody,
Does anybody experienced problems with PVEP coils?
The spool is continuously moving (+/- 50%) with a constant setpoint.
The feedback indicated that the duty cycle is Ok and a similar value as setpoint.

If we use the manual lever instead of a setpoint from the ECU, the flow is continous, about +/-5%.
So manually it is correct, but not with electric setpoint!

May be somebody to help us?

We are going to try the special PVEP function block.

Thanks...

Offline hproffitt

  • PLUS+1 Developer
  • ***
  • Posts: 28
  • Karma: +0/-0
Re: PVE-P
« Reply #1 on: October 18, 2012, 02:28:05 PM »
My mistake.  PVEP is the PWM control.  I originally gave you the voltage coil info.
« Last Edit: October 19, 2012, 02:13:07 PM by hproffitt »

Offline Neil

  • PLUS+1 Expert
  • ****
  • Posts: 96
  • Karma: +2/-0
Re: PVE-P
« Reply #2 on: October 18, 2012, 10:03:57 PM »
Hi.

PVEP characteristics are shown below, I would try pinconfig3.

Neil