PLUS+1 User Forum

PLUS+1 Hardware => Displays => Topic started by: Mike AA on December 11, 2020, 07:11:43 PM

Title: Display Buzzer
Post by: Mike AA on December 11, 2020, 07:11:43 PM
I am looking at the outputs on the DM1200 and data sheet and I don't see if the buzzer is simply an output port or if there is an actual buzzer built into the display. Under buzzer it doesn't give me a port to connect to. I the data sheet there is no discussion of where to connect externally.

Help please?

Mike
Title: Re: Display Buzzer
Post by: A.Fitz on December 11, 2020, 10:24:50 PM
Hey Mike,

Looking at the guide template, looks like the buzzer is built into the display, see attached image.
Title: Re: Display Buzzer
Post by: Mike AA on December 12, 2020, 03:00:35 PM
A.Fitz,

That is exactly what I see and when I enable the buzzer with the default volume and frequency I don't hear anything.

I have my service tool monitoring the signal and it shows I am enabling it.

Mike
Title: Re: Display Buzzer
Post by: Tor on December 14, 2020, 11:51:53 AM
Hi,

No, there is no built in buzzer in the DM1x00. The name on the output is a bit misleading.
Here's a video that explains how to get the "buzzer" and sound going:    https://www.youtube.com/watch?v=Qip8rPAA8mI (https://www.youtube.com/watch?v=Qip8rPAA8mI)

I hope it helps.

Have a nice day.