Author Topic: DP610 - Ever Seen this?  (Read 2342 times)

Offline niteRider

  • PLUS+1 Developer
  • ***
  • Posts: 45
  • Karma: +3/-0
DP610 - Ever Seen this?
« on: January 10, 2020, 02:38:59 PM »
Got the attached back from a customer... unit has been in the field since 2013.  I was able to download the correct application and fix it, but the ECU History doesn't look right... I put a label on the displays when I download the application, and this one shows that I did it on 7/30/2013.  That doesn't line up with the history, though...

This looks like some kind of default screen, like maybe what it looked like before the default Danfoss program was loaded?

Weird.

Offline G30RG3

  • PLUS+1 Expert
  • ****
  • Posts: 71
  • Karma: +3/-0
Re: DP610 - Ever Seen this?
« Reply #1 on: January 13, 2020, 09:14:46 AM »
Since the Application file name is the earliest version, I would guess this is what you see in a Boot Loading application