PLUS+1 Software > Telematics

CAN informations view

(1/2) > >>

Loader:
Hi, is there a method to view the messages on CAN bus? For example like CanKing?
Thanks!

spittet:
Why not use CANKing? It's designed exactly for this.

Sam

Loader:
Hi Spittet, when I use Telematic hardware I don't see anything on CAN bus with CANKing!!
I something wrong?
Thanks

spittet:
Ok, I didn't see that this post was related to Telematic. I have no clue on this one. Sorry.

Sam

jashom1:
I have viewed Telematics data and Service tool data with CanKing and the CG150.

All you have to do is in the CAN Controller window under the Bus Parameters tab, un-tick "Exclusive" and tick "No init access" This then does not configure the CG150 to communicate but relies on the main program wether it's the Service Tool, or the Telematics configurator.  The catch here is you won't see anything until the service tool or Telematics configurator configures the CG150 for communication.

With this method you still can send messages too

I use it all the time.

Navigation

[0] Message Index

[#] Next page

Go to full version