PLUS+1 Tools > PLUS+1 Service Tool
E270: Invaild data in file.....
(1/1)
PARK HAN SOO:
Any body knows what this error means, and how to solve it?
I can't open the service tool file. :-X :-X :-X
acmall:
This could be cased by this issue.
[P100007144] P1D files saved in 2024.2.4 could not be opened by a user of older Service Tools that also used an old version of P1 Base.
If you open the Update Center it should pop up a message that there is new version of the Update Center. This will also update P1 Base.
PARK HAN SOO:
It opens on my computer, but not on other computers with the same version of the service tool installed.
acmall:
It is not the version of the Service Tool that you are using to open the file that causes the issue I posted, it is the version of P1 Base.
We had the exact same issue you are describing and it was resolved by updating the Update Center which also updates P1 Base. After doing this the file could be opened in the same version of the Service Tool that was previously giving the error.
PARK HAN SOO:
Thank for your reply.
I solved the problem. Thank you. :D :D :D :D
Navigation
[0] Message Index
Go to full version