PLUS+1 Hardware > PLUS+1 CS Hardware
CS100 CONFIGURATION AT PORTAL
(1/1)
pinias:
Hi Guys,
this is the first time I will be using a CS100, still waiting for the device but in the mean time I tried to do a simple configuration for it on the PLUS1 Connect portal.
when trying to do it I had few errors, is that becuase the device is not added on the PLUS 1 Connect portal yet?
see screen shots, basically it does not accept the CAN ID I want to work with, not sure what multiplier means, it asks for ID Mask but it is 11 bit only CAN ID.
does anyone can advise about
thank you
pinias:
Just an update about
we are 2 administrators of the portal, so both should be able to create and modify the configuration files, however for some reason just my colleage can do that, if I try to do it, it seems to work until I hit the save/create button, basically it saves no any changes I made. we have compared all adminstrator settings and both are the same..kind of odd this issue.
Regards
Navigation
[0] Message Index
Go to full version