Author Topic: DST X5 J1939 Template  (Read 12 times)

Offline sanjeewa

  • PLUS+1 Novice
  • *
  • Posts: 1
  • Karma: +0/-0
DST X5 J1939 Template
« on: Today at 03:49:26 PM »
Hi,

I am trying to utilize DST X5 J1939 Hardware template to get angle from DST X520 rotary sensor and having issue with the output.
It is not outputting angle and showing message is not received when I check the checkpoint.
However, I have used CAN message decoding component to decode receiving DST x520 message 18FF0B15.
I can see that message is receiving in the same CAN interface where I have connected the template block.

Can someone please help me to figure it out?




Thanks