Recent Posts

Pages: 1 2 3 [4] 5 6 ... 10
31
PLUS+1 Service Tool / Canalyser VN1610 instead of Danfoss gateway
« Last post by Thierry_ACE_germany on June 20, 2024, 04:15:38 PM »
Hello ,

For E-steering i only want to use Vector Cananlyser , how can i make it visible in service tool  instead of our Kvaser gateway ?

thanks Thierry
32
Function Library / DST X5 J1939 Template
« Last post by sanjeewa on June 20, 2024, 03:49:26 PM »
Hi,

I am trying to utilize DST X5 J1939 Hardware template to get angle from DST X520 rotary sensor and having issue with the output.
It is not outputting angle and showing message is not received when I check the checkpoint.
However, I have used CAN message decoding component to decode receiving DST x520 message 18FF0B15.
I can see that message is receiving in the same CAN interface where I have connected the template block.

Can someone please help me to figure it out?




Thanks
33
Displays / Re: download file via USB Host
« Last post by Marbek_Elektronik on June 11, 2024, 12:16:00 PM »
But it is not USB-Host. USB Host is the same Pin as RS232. Here you can connect an USB stick. I will try it today....
34
Displays / Re: DM700 portrait layout or vertical layout
« Last post by Link on June 10, 2024, 08:47:39 AM »
In addition to what Acmall said, in the update center under "Training Video Extras" there is a example project called: "DM1000 Application Example". This example project also has an example of how to switch between Horizontal and Vertical.
35
Displays / Re: DM700 portrait layout or vertical layout
« Last post by acmall on June 10, 2024, 08:42:39 AM »
In the VBSE Screen Manager panel click on the top level to select it (should be the name of your screen definition). Then in the Inspector panel expand Top Level and you will see rotation.
36
Displays / Re: DM700 HWD FILE
« Last post by pinias on June 09, 2024, 12:51:56 AM »
FYI

the issue was the Plus1 GUIDE version I was working with it has to be 2023 or later otherwise it just does not load up the HWD for DM700

Thanks

 ;D
37
Displays / DM700 portrait layout or vertical layout
« Last post by Beezkneez on June 08, 2024, 12:31:39 AM »
I am trying to find a setting in the vector based screen editor to flip the display orientation from horizontal to vertical or landscape to portrait. I am not finding it. I searched the manual and still not finding what I am looking for. I’m hoping it’s something simple that I am overlooking. Has anyone done this? Used a screen in a vertical position instead of horizontal or portrait instead of landscape?
38
Displays / Re: Data logging limitation
« Last post by Mike AA on June 04, 2024, 09:13:59 PM »
LUKEY,

Thanks for the examples again! I figured you through into an array and this will all work perfectly for our uses. I have to change a few things but it should all work out. Arrays and Strings, a great way to put a whole lot of data in a small space.
39
Displays / Re: Bug in Screen Editor
« Last post by williamk on June 04, 2024, 09:04:11 PM »
After some troubleshooting, I was able to solve the issue.  I had some a Line object within the widget which had default start and end points were at the same X,Y coordinates (I was planning on changing the Begin Point X value to something else based on data being fed into the widget). 

I'm not sure why this causes the widget to collapse when it's used in another screen and resized but changing the initial values to no longer be on top of one another fixed the problem.
40
Displays / Re: Data logging limitation
« Last post by Lukey on June 04, 2024, 02:32:40 AM »
Ah I didn't realise CONCAT was limited to 16, I guess the work around is to then run two POUS and CONCAT two strings together again and so on as required.

See attached my date time page.
Pages: 1 2 3 [4] 5 6 ... 10