PLUS+1 User Forum
PLUS+1 Tools => PLUS+1 Service Tool => Topic started by: williamk on January 24, 2022, 11:51:08 PM
-
Occasionally I will get an error with the text: "Error: Download transfer timeout" and Download Status: "E266: Download transfer timeout".
Is there some way to increase the timeout? I've seen this error while using a PEAK adapter in RP1210C mode and while using a Kvaser Leaf Light. In both instances, the display (DM430E) and the adapter were the only things connected to the CAN bus and the bus had proper terminating resistors.
-
Hello!
Have you found the solution to this problem, as we are experiencing almost the same thing here.
Regards,
Nikola.
-
I don't know the reason but I also have problems with ServiceTool and PEAK-Interface.
Therefore I only use the Danfoss CG150-2 for the ServiceTool.
PCAN-View with PEAK interface to investigate CAN messages, I never use Danfoss CAN-King as it is buggy.
-
I don't know the reason but I also have problems with ServiceTool and PEAK-Interface.
Therefore I only use the Danfoss CG150-2 for the ServiceTool.
PCAN-View with PEAK interface to investigate CAN messages, I never use Danfoss CAN-King as it is glitchy.
Fredrick, what do you mean CAN-King is glitchy?
-
Ok, maybe I used the wrong word for it ;)
CAN-King does not work for me, the program freezes or stops behaving normally after a while.
PCAN View always works and you can use both ServiceTool and PCAN View at the same time.
Yes, I know that you can do that with CAN-King as well if you configure it right.