Author Topic: J1939 w/ Tier4 Final Supported PGNS  (Read 11327 times)

Offline niteRider

  • PLUS+1 Developer
  • ***
  • Posts: 45
  • Karma: +3/-0
J1939 w/ Tier4 Final Supported PGNS
« on: February 04, 2014, 05:59:33 PM »
I need DEF related PGN support, specifically:

PGN 64821 SPN 4427 (DEF Tank Temp)
PGN 65110 SPN 1761 (DEF Tank Level)
PGN 64923 SPN 3616 (DEF Quality)

Has anyone heard if Danfoss plans on updating the J1939 Function Library?
« Last Edit: February 05, 2014, 11:49:10 PM by niteRider »

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
Re: J1939 w/ Tier4 Final Supported PGNS
« Reply #1 on: April 23, 2014, 11:17:43 PM »
You can use the Recieve CAN block just make sure EXT is set to true.

 See file attached in regards of the PGN information

Good luck


Offline niteRider

  • PLUS+1 Developer
  • ***
  • Posts: 45
  • Karma: +3/-0
Re: J1939 w/ Tier4 Final Supported PGNS
« Reply #2 on: April 24, 2014, 09:11:18 PM »
Thanks... I ended up just writing it myself.  See here:
http://www.plus1forum.danfoss.com/index.php?topic=660.0

bgtwuk

  • Guest
Re: J1939 w/ Tier4 Final Supported PGNS
« Reply #3 on: April 25, 2014, 09:17:29 PM »


Nite Rider rocks.....

Bgtwuk

Offline Jakob

  • PLUS+1 Expert
  • ****
  • Posts: 98
  • Karma: +2/-0
Re: J1939 w/ Tier4 Final Supported PGNS
« Reply #4 on: May 02, 2014, 08:35:22 AM »
Where is the LIKE button  ;)