Author Topic: Rs232 to Can Converter  (Read 6858 times)

Offline F.M.Elettromeccanica

  • PLUS+1 Developer
  • ***
  • Posts: 47
  • Karma: +1/-0
Rs232 to Can Converter
« on: May 17, 2020, 06:08:20 PM »
Hallo guys,
Anyone who knows how an rs232 to Canbus converter works?
I wish to acquire an NMEA input in serial format and convert it in some can messages.
Is there a device that do it?

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 220
  • Karma: +7/-0
Re: Rs232 to Can Converter
« Reply #1 on: May 21, 2020, 05:53:24 PM »
Hey F.M. E

I have used the EATON XC152 PLC, basically interfacing RS485 with CAN 2.0A, for the danfoss displays but it also comes with RS232 , I would say that the only downside is that you need to know structured text or at least for me it was easier than other methods.

I tried some other gateways from anybus or so but for some reason I could not make it work.

I hope this helps

Regards

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 197
  • Karma: +37/-1
Re: Rs232 to Can Converter
« Reply #2 on: May 22, 2020, 09:25:57 AM »
If you have a Danfoss display in your system check it first as some of the Danfoss displays have RS232 capability. We use a receipt printer over RS232 connected to a DP720.

Also check Peak System https://www.peak-system.com. I have not used it but I believe they may have a convertor.