Author Topic: Kvaser BlackBird SemiPro HS  (Read 21086 times)

itec-electronics

  • Guest
Kvaser BlackBird SemiPro HS
« on: April 04, 2011, 07:43:36 PM »
Hi Plus+1 People,

Has anybody tried to use the Kvaser BlackBird SemiPro HS with Guide?  It is a CAN dongle that connects to your PC using wi-fi, hence no wires tying you to the machine.

Would be great if it works, but too expensive to buy one without knowing.

Thanks, Ian.

Martin s.

  • Guest
Re: Kvaser BlackBird SemiPro HS
« Reply #1 on: December 03, 2014, 09:31:42 AM »
Yes it works, i use it my self! Range is about 200-300 meter in free air. Using the servicetool the updatetime  is from 5- 20 msec depending on number of checkpoints :-)

Regards Martin

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 352
  • Karma: +8/-0
    • Marbek Elektronik
Re: Kvaser BlackBird SemiPro HS
« Reply #2 on: February 20, 2015, 10:44:52 AM »
Is this the best gateway to use?
I am using CG150 and USB, in case of DPXXX.

Whats about download time, service tool update time, costs, easy to hand ?
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline hgb1992

  • PLUS+1 Developer
  • ***
  • Posts: 13
  • Karma: +0/-0
Re: Kvaser BlackBird SemiPro HS
« Reply #3 on: March 11, 2015, 11:57:09 AM »
Hi guys!

We are normally use CG150 and USB but especially for H1AC applications (Parameter Setting) we work with Kvaser Black Bird Semi Pro.

Down- und Upload-Performance are nearly compareable to CG150.
Easy to handle, but you need administration rights on your notebook for the wireless settings.

KR, Benedikt

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 352
  • Karma: +8/-0
    • Marbek Elektronik
Re: Kvaser BlackBird SemiPro HS
« Reply #4 on: March 11, 2015, 03:45:03 PM »
Hi,
does it works fine by:
- dowload files with service-tool?
- download and upload parameters with service - tool?
- watching chekcpoints, trigger inputs with service-tool?

- logging and playing data with Kvaser software?

If you say yes to all 4 points, I will buy this!
Where have you buyed it and what price is it?

Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung