Recent Posts

Pages: 1 ... 8 9 [10]
91
PLUS+1 Service Tool / Re: File Download Failed
« Last post by sverreo on June 08, 2023, 09:35:36 PM »
I don't know the reason but I also have problems with ServiceTool and PEAK-Interface.

Therefore I only use the Danfoss CG150-2 for the ServiceTool.
PCAN-View with PEAK interface to investigate CAN messages, I never use Danfoss CAN-King as it is glitchy.

Fredrick, what do you mean CAN-King is glitchy?
92
PLUS+1 Service Tool / Re: File Download Failed
« Last post by Fredrick on June 08, 2023, 05:48:30 PM »
I don't know the reason but I also have problems with ServiceTool and PEAK-Interface.

Therefore I only use the Danfoss CG150-2 for the ServiceTool.
PCAN-View with PEAK interface to investigate CAN messages, I never use Danfoss CAN-King as it is buggy.
93
PLUS+1 News / Re: Danfoss Account Login issue.
« Last post by Tor on June 08, 2023, 02:30:03 PM »
Hello,

News about the issue:
"There is currently a problem with our Danfoss Identity Provider (DIP).
This issue is currently preventing all login attempts through the PLUS+1 Update Center. Therefore, you should currently refrain from logging out of the PLUS+1 Update Center, as a later attempt to log in will not work.
This issue currently affects the PLUS+1 Update Center and Remote InterLink login via PLUS+1 Service Tool.

The issue has been identified and fixed, and a patch will be released as soon as possible for the Update Center and the Service Tool.

Please contact the helpdesk if you need data, documents, or other attachments that you normally receive from the PLUS+1 Update Center."


There is also a "work around" identified.  - Note! This didn't work for me, but for some of my colleagues - :

"Without closing the White popup window if you right click on the icon in the task bar you can open the PLUS+1® Update Center window.  See image.

When this window is open (It will indicate there are no subscriptions ) if you press F5 the software looks like it is scanning the subscriptions, there is a “hide” button that needs to be pressed.
This closes out the Update Center window and you get a popup indicating the PLUS+1 Update Center is still running.
If you then again right click on the icon in the Windows Task bar (this icon remains in spite of the previous popup) it looks like the subscriptions are now populated."


I hope it helps some of you. If not, I hope the patch will be released soon.


Have a nice day.





94
PLUS+1 News / Re: Danfoss Account Login issue.
« Last post by Tor on June 08, 2023, 08:03:30 AM »
Hello,

Yes it is still an issue. 
They have found the problem and are looking for a way to fix it.  Somehow there have been a change in the DIP (Danfoss Identity Provider) that have caused the issue.

I will post more information as soon as possible.
95
PLUS+1 News / Re: Danfoss Account Login issue.
« Last post by deaks57 on June 08, 2023, 07:01:25 AM »
Hi Tor, is this still a problem? I have a customer with issues.
Cheers
96
PLUS+1 News / Danfoss Account Login issue.
« Last post by Tor on June 07, 2023, 03:10:42 PM »
Hello,

There seems to be an issue with the Danfoss Account (DIP) that makes it impossible to log in again after logging out.
This has been reported when using the PLUS+1 Update Center, but other tools are affected as well.

So, if you are logged in, don't log out, and you will be fine.
The developers are trying to find a solution and I hope it will be solved soon.

Thank you
97
PLUS+1 Service Tool / Re: File Download Failed
« Last post by vnikola on June 07, 2023, 09:30:28 AM »
Hello!

Have you found the solution to this problem, as we are experiencing almost the same thing here.


Regards,
Nikola.
98
Function Library / Re: CANopen function block library
« Last post by deaks57 on June 05, 2023, 11:35:36 PM »
Ignore that, pilot error.
99
Function Library / CANopen function block library
« Last post by deaks57 on June 05, 2023, 10:28:38 PM »
Has anyone got an example p1p to successfully drive a series 5 PVED?
I can't even get the green LED to light (PVED is mounted to PVB)
100
PLUS+1 GUIDE / Re: Hardware configuration (EDF file)
« Last post by Daan on June 02, 2023, 08:11:07 AM »
Hety Deaks57

EDS files are simple text files used by network configuration tools to help you identify products and easily commission them on a network.
But since I can't really find anything about this in PLUS+1 Guide I'm probably going to have to hardcode it.

Hopefully you now understand what I mean by an EDS file.  :)

Update: My mistake, it's an EDS file
Pages: 1 ... 8 9 [10]