Author Topic: Curved Monitor usefull ?  (Read 2490 times)

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Curved Monitor usefull ?
« on: December 21, 2023, 07:37:14 PM »
Hi,
I have a HP 30" Monitor.
I am thinking about curved monitor as computer players use.

Does anyone use such a monitor?

I think, the plane one is better than a curved one.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Lukey

  • PLUS+1 Developer
  • ***
  • Posts: 49
  • Karma: +5/-0
Re: Curved Monitor usefull ?
« Reply #1 on: December 22, 2023, 03:23:40 AM »
Cured monitors I think they are overrated/a gimmick, personally I use 3x 27".

Great for multi tasking, for example viewing, Guide, service tool and a data sheet

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 278
  • Karma: +27/-1
Re: Curved Monitor usefull ?
« Reply #2 on: December 22, 2023, 07:59:31 AM »
Hello,

Can we keep this as a discussion if curved monitors are useful when developing in PLUS+1 GUIDE I will keep it here. In other cases I will move it to the "Off Topic" section.

For GUIDE developing I believe it can be a good thing. Large drawing on the screen, and everything at the same distance to your eyes. Your eyes don't have to re-focus as much when you are turning your head?  This is what I think, I don't have any facts to back me up.

The curved monitor has become a standard in our office, but myself are using two 27" flat monitors and a laptop screen. I thought it got a little crowded running both Service Tool and GUIDE on the same monitor. And if I wanted the same setup as I have now, I would have to get a 49" curved monitor (If I remember correct) and that was not an option.


Have a nice Holiday.
Best regards,
Tor
PLUS+1® SW PAE Team