Author Topic: DM700 HWD FILE  (Read 5860 times)

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 220
  • Karma: +7/-0
DM700 HWD FILE
« on: May 30, 2024, 02:59:59 PM »
Hey Guys,


Do you know where can I get the DM700 HWD file?

My Plus1 update center does not show it

Thank you

 :)


Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 296
  • Karma: +28/-1
Re: DM700 HWD FILE
« Reply #1 on: May 31, 2024, 07:57:11 AM »
Hello Pinias,

It's in there.  See attached image.


Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 220
  • Karma: +7/-0
Re: DM700 HWD FILE
« Reply #2 on: May 31, 2024, 02:25:04 PM »
Hi Thor.

well, my +1 update center has that missed

see attached picture of the version I got

I appreciate any feedback about

Regards


Offline Link

  • PLUS+1 User
  • **
  • Posts: 9
  • Karma: +0/-0
Re: DM700 HWD FILE
« Reply #3 on: May 31, 2024, 04:24:57 PM »
Hello Pinias,

That means you're already "subscribed" to these updates, if you look in the top right you see your active subsriptions, with an edit button.
Press that edit button and search for the DM700 HWD files.

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 220
  • Karma: +7/-0
Re: DM700 HWD FILE
« Reply #4 on: May 31, 2024, 06:16:29 PM »
Hey JordyHV

ok, that is in the subscribed list

the questions is why is it not available for download and get it installed on the +1 GUIDE?

do I need the latest version of guide to get it available for download? not sure I have been able to work with the DM1XXX with older versions of GUIDE
 
if I modify my subscriptions leaving the DM700 only and save that then I got nothing for download. :'(

 have you tried to get it available for download? did it work? what version of guide are you working with?

Thank you

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 296
  • Karma: +28/-1
Re: DM700 HWD FILE
« Reply #5 on: June 03, 2024, 08:03:33 AM »
Hello pinias,

Make sure that it's not already installed.
If you have subscribed to the files and it doesn't show up in the download list it's probably already installed.
Have a look in the hardware tab in PLUS+1 GUIDE. If you don't see it take look in the download folder for Update Center if the file is there. Search for DM700.


Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 220
  • Karma: +7/-0
Re: DM700 HWD FILE
« Reply #6 on: June 09, 2024, 12:51:56 AM »
FYI

the issue was the Plus1 GUIDE version I was working with it has to be 2023 or later otherwise it just does not load up the HWD for DM700

Thanks

 ;D