Author Topic: Bug?  (Read 3919 times)

Offline Undertow

  • PLUS+1 Developer
  • ***
  • Posts: 21
  • Karma: +0/-0
Bug?
« on: October 17, 2011, 03:30:22 PM »
Hi,
Just wanted to point out something that could be an issue.
While compiling an application I tried to stop the compile so I could add something I forgot about, I clicked the Break button and Microsoft Office completely crashed.
The only way to get it back was to restart the computer but all office programs had closed straight away, didn't lose anything thankfully but that was just luck.
I don't think the issue is on the computer side as its spec is pretty good I am convinced this was something coming from breaking the compile.
Maybe the break buttons function is to Break Office  :D
Is this the section where we should highlight bugs or should there be a spacific location?

Offline Stefan

  • Administrator
  • PLUS+1 Expert
  • *
  • Posts: 72
  • Karma: +0/-0
Re: Bug?
« Reply #1 on: October 24, 2011, 02:33:22 PM »
Hello,

Please send bugs to helpdesk@sauer-danfoss-plus1.com.


Best regards
Stefan Arvidsson