PLUS+1 Software > Communication
how is virtual CG150 ?
tronelec:
Hi guys, what is it for and what use can be made of virtual danfoss CG150 virtual ??
FluidPowerTom:
This sort of came up recently in a discussion with Danfoss, and my recollection is that there's virtually no use for the virtual CG-150 (pun intended). We asked them to remove this entirely. I get calls regularly - this week included - from customers who's Service Tool is mistakenly looking at the virtual CG-150. It just needs to be removed ASAP please Danfoss.
Tor:
Hi,
Now I'm curious.
I can't remember any time I have ever used this virtual channels in Service Tool. But they are probably there for a reason?
I will try to get some answers from the developers and see if I can get some history on these virtual channels. If they are not necessary, and cause confusion, it might be a good idea to remove them.
Unfortunate it's vacation time, and it may take a while, but I will keep you posted whenever I get an answer.
Have a nice day.
tronelec:
buuuu :o, I thought it is for hardware simulation, this I need especially when it is a system with more than one controller, IQAN has it more than covered many years ago
FluidPowerTom:
--- Quote from: tronelec on July 14, 2020, 05:23:14 AM ---buuuu :o, I thought it is for hardware simulation, this I need especially when it is a system with more than one controller, IQAN has it more than covered many years ago
--- End quote ---
I'm going to resurrect this topic. Can anyone confirm if the CG-150 is actually used for some kind of simulation? If it has no real use it should be on the chopping block, as it is a frequent cause of phone calls from technicians in the field.
Navigation
[0] Message Index
[#] Next page
Go to full version