Author Topic: Applog size and memory usage  (Read 1951 times)

Offline Lukey

  • PLUS+1 Developer
  • ***
  • Posts: 49
  • Karma: +5/-0
Applog size and memory usage
« on: February 29, 2024, 06:35:03 AM »
Hello, i am using a DM1200T.

Is there anyway to ready the 32mb applog memory size to determine how much has/is being used?

Reading the OS.RAM and OS.Flash values indicates that the applog memory usage has no influence on these values, as I cannot see an significant changes when writting/reading to the applog memory.

The Write_USB block (designed for the DP720 does not work with this hardware fully) does not give information on Used_Blocks or Free_Blocks unfortunately.