PLUS+1 Hardware > Displays
USB stick on display?
(1/1)
Quax76:
Hi everybody,
is there a chance to connect an usb-stick to one of the available displays to write machine configuration data on it?
What I would like most is to use DP610 and connect a USB connector to the 7 pin Binder connector (C3).
If this doesn't work, could I use the DP210 with front USB (using application data kogging)?
Thanx!
Stefan:
Hello,
There are plans to implement components that can extract the data from an Application logg and send it to the USB-port but it's not available yet. Unfortunately I can give you any date when it will be released.
Stefan
Navigation
[0] Message Index
Go to full version