But whats about driving PVEH at voltages at 10V (machine starting for example)?
At 24V you have 0,3A, at 12V: 0,57A, at 10V: 0,7A (10Watt) !
Now, if you drive 5 PVEHs, the current will be 3,5A, which is to big!
I think, you must not drive more then 4 PVEHs on a digital output PIN.
PVEA will be no problem because of lower current.
Is this OK?