PLUS+1 Hardware > PLUS+1 Compliant Hardware
JS1H - Digi out
(1/1)
magitec:
Hi,
I have a JS1H with 2 buttons, one on the top and one on the shaft (OP present) on the wiring pinout i have on the black connector a Dig out 1 and Dig out 2.
i am feeding 12v to pin 2 (pwr 1) and gnd to pin 1. on the grey connector.
* So do the dig out 1 and 2 output 12v+ when the button is pressed?
* do i also need to add 12v to Pwr 2, Pwr 3 and Pwr 4 too?[/li]
[/list]
many thanks.
FluidPowerTom:
It looks like it's a yes on all accounts
magitec:
Perfect thank you. just a few other questions i'm using the PMW output for a 12v reversible output to control a 12v actuator forward is 0 - 12v and then backwards is 12 - 0v which PID file do i require for setting up the limits / proportional control scale.
again thank you, its not something i have used before, i do have the correct CG150-2 cable
Navigation
[0] Message Index
Go to full version