Recent Posts

Pages: 1 [2] 3 4 ... 10
11
Controllers / Re: use MC50 and IOX24 together
« Last post by Marbek_Elektronik on January 25, 2022, 01:48:57 PM »
See here
12
Controllers / Re: use MC50 and IOX24 together
« Last post by Marbek_Elektronik on January 25, 2022, 01:48:21 PM »
(Perhaps you find a newer document)

The can_config of Module is important:
In example I have NodeID=0
13
Controllers / Re: use MC50 and IOX24 together
« Last post by Marbek_Elektronik on January 25, 2022, 01:40:54 PM »
and this
14
Controllers / Re: use MC50 and IOX24 together
« Last post by Marbek_Elektronik on January 25, 2022, 01:40:22 PM »
Here an example:
15
PLUS+1™ Service Tool / Re: Monitoring inputs
« Last post by acmall on January 25, 2022, 09:35:07 AM »
There is no monitoring/debugging mode like you will find on some other systems. To monitor values you use the Plus+1 Service Tool.

There are a number of pre-configured signals including all the I/O pins. For any other values in your program that you want to monitor you need to add checkpoints.

If you are not familiar with the Service Tool this video may help.
https://www.youtube.com/watch?v=sEfS7sU33eY&list=PL6wa1HRpyb0TppKA4w3fNSYGbQvnxgBVd&index=10
16
Controllers / use MC50 and IOX24 together
« Last post by topal on January 25, 2022, 07:51:55 AM »
Hello,

I would need to know if when using an IOX24 module with an MC50-110n controller it is mandatory to use the SUB-CMDs of the IOX24 module for my program which is in my MC50 or else I can directly use the name of the IOX24 input?

because when I use the name of the inputs directly it does not work

and when I want to use SUB-CMd it's me who doesn't understand how to use these commands

could you help me ?

thank you

Pat
17
PLUS+1™ Service Tool / File Download Failed
« Last post by williamk on January 24, 2022, 11:51:08 PM »
Occasionally I will get an error with the text: "Error: Download transfer timeout" and Download Status: "E266: Download transfer timeout".

Is there some way to increase the timeout?  I've seen this error while using a PEAK adapter in RP1210C mode and while using a Kvaser Leaf Light.  In both instances, the display (DM430E) and the adapter were the only things connected to the CAN bus and the bus had proper terminating resistors.
18
Controllers / Re: Hydrostatic pump controller
« Last post by deaks57 on January 24, 2022, 11:00:23 PM »
@matttargett4 Yes 24V is fine.
19
PLUS+1™ Service Tool / Monitoring inputs
« Last post by matttargett4 on January 21, 2022, 08:28:36 PM »
Hi,

I’m building a basic application and to verify it’s working correctly I would like to be able monitor how inputs and outputs vary as I adjust connected hardware, in my experience with other plc stuff there is usually a monitoring mode where you can simply see your program and how it behaves in real time.

Is there something like this I can do? Or some other way of achieving what I’m after?

Thanks

Matt
20
Controllers / Re: Hydrostatic pump controller
« Last post by tronelec on January 21, 2022, 06:06:53 PM »
in my experience the problem will be the other way around if the actuator is 24 volt and your source is 12 volt, but the actuators for pumps consume very little current, if you don't over do the current there would be no problem, what if the curve changed relationship between current versus flow
Pages: 1 [2] 3 4 ... 10