PLUS+1 Software > Communication
Use PEAK-to-USB for Plus+1 service tool
Morten Rosengreen:
Thanks for reply
Did you manage to find the correct file?
I have tried, but could see the log for the RP1210:
Parse results for: C:\WINDOWS\RP121032.INI:
--PEAKRP32
Parsing: PEAKRP32
Parse results for: C:\WINDOWS\PEAKRP32.ini:
Name: PEAK-System PCAN Adapter
Address1: Otto-Roehm str. 69
Address2: (Not specified)
City: Darmstadt
Country: Germany
State: Hessen
Postal: 64293
Telephone: 0049-6151-817320
Fax: 0049-6151-817329
VendorURL: http://www.peak-system.com
Version: 3.0
RP1210 Version: C
*** WARNING *** [C:\WINDOWS\PEAKRP32.ini] Gateway uses C. PLUS+1 Service Tool is tested with RP1210A and RP1210B.
CANFormatsSupported: 3,4,5
Protocols: 10,20,30
Devices:
C:\WINDOWS\system32\PEAKRP32.dll exported functions:
ClearRegisteredDevices
GetLicenseInfo
GetLicenseStatus
RP1210_ClientConnect
RP1210_ClientDisconnect
RP1210_GetErrorMsg
RP1210_GetHardwareStatus
RP1210_GetLastErrorMsg
RP1210_Ioctl
RP1210_ReadDetailedVersion
RP1210_ReadMessage
RP1210_ReadVersion
RP1210_SendCommand
RP1210_SendMessage
RegisterAttachedDevices
RegisterPEAKRP1210
RegisterRPDevice
UnregisterPEAKRP1210
UnregisterRPDevice
--
Attempting to add protocol: 10
Protocol: 10
ProtocolDescription: CAN Network Protocol
ProtocolString: CAN
ProtocolSpeed: 125,250,500,1000,Auto
ProtocolParams:
Devices:
*** SKIPPED *** This protocol has no useable devices!
Failed to add protocol: 10
--
Attempting to add protocol: 20
Protocol: 20
ProtocolDescription: SAE J1939 Protocol
ProtocolString: J1939
*** SKIPPED *** "ProtocolString" must be CAN
Failed to add protocol: 20
--
Attempting to add protocol: 30
Protocol: 30
ProtocolDescription: ISO15765 Vehicle Protocol
ProtocolString: ISO15765
*** SKIPPED *** "ProtocolString" must be CAN
Failed to add protocol: 30
*** WARNING *** [C:\WINDOWS\PEAKRP32.ini] Generic CAN protocol is not supported.
--
Attempting to add protocol: 10
Protocol: 10
ProtocolDescription: CAN Network Protocol
ProtocolString: CAN
*** SKIPPED *** "ProtocolString" must be J1939
Failed to add protocol: 10
--
Attempting to add protocol: 20
Protocol: 20
ProtocolDescription: SAE J1939 Protocol
ProtocolString: J1939
ProtocolSpeed: 125,250,500,1000,Auto
ProtocolParams:
Devices:
*** SKIPPED *** This protocol has no useable devices!
Failed to add protocol: 20
--
Attempting to add protocol: 30
Protocol: 30
ProtocolDescription: ISO15765 Vehicle Protocol
ProtocolString: ISO15765
*** SKIPPED *** "ProtocolString" must be J1939
Failed to add protocol: 30
*** ERROR *** [C:\WINDOWS\PEAKRP32.ini] No valid protocols (The Generic CAN or J1939 protocol is needed by PLUS+1 Service Tool)
Failed to parse: C:\WINDOWS\PEAKRP32.ini
*** WARNING *** No RP1210 vendor files parsed successfully
Navigation
[0] Message Index
[*] Previous page
Go to full version