Author Topic: Shortcuts  (Read 4846 times)

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Shortcuts
« on: April 11, 2015, 04:30:24 PM »
Hi,
The Guide shortcut menue is not very comfortable.

Specially I want to add a shortcut for going forward or backward.
In classic shortcuts we use Alt+Arrow left, right,
but I want to use the mouse forward/backward-key,
because I don't want to take my right hand from mouse to keyboard.
Does anyone knows how to do this?

Thanks in forward,
Bernd
« Last Edit: April 11, 2015, 05:17:21 PM by Marbek_Elektronik »
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline oiltronic

  • PLUS+1 Guru
  • *****
  • Posts: 170
  • Karma: +15/-0
Re: Shortcuts
« Reply #1 on: April 14, 2015, 07:11:52 AM »
That's a good idea.  So I tried setting up application-specific keyboard macros in my Microsoft mouse setup, so that the forward mouse button is 'E' and the back mouse button is 'L'.  Unfortunately the macros had no effect, even after restarting GUIDE.  It seems that GUIDE forces these buttons to next & previous page.

Offline BRIan

  • PLUS+1 Expert
  • ****
  • Posts: 56
  • Karma: +3/-0
Re: Shortcuts
« Reply #2 on: April 15, 2015, 01:11:59 AM »
Custom keyboard shortcuts are already handled in GUIDE (see attached) but I don't know how you could add mouse inputs.

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Shortcuts
« Reply #3 on: April 15, 2015, 11:34:34 PM »
But there are not all commands.

For example: "F9" to abort routing, previous page, next page,.....

This table should be complete.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung