PLUS+1 Hardware > Displays
Simulator
Stefan:
Hello,
Identity in the Service Tool:
Screen capture from the API Specification regarding Identity of a DP6xx unit:
In the Miscellaneous column you will find the default setting you get if these signals is not drawn in the graphical code. The default settings in the Operating system are the same as the one in the Template, so that's why you don't have to put them back.
These signals gives you the opportunity to select different net numbers.
Example how the Identity is defined:
Service Tool connected to CAN[1] on the display and ID.Net[1].Addr is set 1 and ID.Node.ServerAddr (also called node number) is set to 9 will give you the Service Tool ID 1,9.
Best regards
Stefan
radioact:
Very Interesting,
Thank you for the explanation.
Tyler
Navigation
[0] Message Index
[*] Previous page
Go to full version