PLUS+1 Software > Displays
Real Time Clock For DM430
BBarry:
Thanks Tor for the quick response.
I did that and it did not work.
Where can I check to see if I have the latest HWD file?
Tor:
Hello,
You can see what HWD you have in the Project manager, (#1 in the image).
If it's not 170, go to the Update Center and make sure you have that unit selected in your subscription (#2 in the image).
When you have selected that you'll get these notifications in the Update Center (#3 in the image) when there's a new HWD. Also, the HWD text in GUIDE will turn read if there is a new HWD file you subscribe on.
If the HWD is fine, I guess you have an issue with the logic. The image you posted doesn't show much.
In the second image is my small test logic for the RTC.
I hope it can help.
Navigation
[0] Message Index
[*] Previous page
Go to full version