Author Topic: Display Buzzer  (Read 1195 times)

Offline Mike AA

  • PLUS+1 Guru
  • *****
  • Posts: 109
  • Karma: +0/-0
    • Dewind Dewatering
Display Buzzer
« on: December 11, 2020, 07:11:43 PM »
I am looking at the outputs on the DM1200 and data sheet and I don't see if the buzzer is simply an output port or if there is an actual buzzer built into the display. Under buzzer it doesn't give me a port to connect to. I the data sheet there is no discussion of where to connect externally.

Help please?

Mike

Offline A.Fitz

  • PLUS+1 Novice
  • *
  • Posts: 3
  • Karma: +0/-0
Re: Display Buzzer
« Reply #1 on: December 11, 2020, 10:24:50 PM »
Hey Mike,

Looking at the guide template, looks like the buzzer is built into the display, see attached image.

Offline Mike AA

  • PLUS+1 Guru
  • *****
  • Posts: 109
  • Karma: +0/-0
    • Dewind Dewatering
Re: Display Buzzer
« Reply #2 on: December 12, 2020, 03:00:35 PM »
A.Fitz,

That is exactly what I see and when I enable the buzzer with the default volume and frequency I don't hear anything.

I have my service tool monitoring the signal and it shows I am enabling it.

Mike

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 179
  • Karma: +15/-1
Re: Display Buzzer
« Reply #3 on: December 14, 2020, 11:51:53 AM »
Hi,

No, there is no built in buzzer in the DM1x00. The name on the output is a bit misleading.
Here's a video that explains how to get the "buzzer" and sound going:    https://www.youtube.com/watch?v=Qip8rPAA8mI

I hope it helps.

Have a nice day.
Best regards
Tor
PLUS+1 Helpdesk team