Author Topic: CANopen Master  (Read 5673 times)

NickFro

  • Guest
CANopen Master
« on: May 12, 2014, 03:55:06 PM »
I am having a problem initiating the communication with a CANopen device from my MC050-020.  The device displays an error message stating "Waiting for NMT-START telegram from CAN master."  I have tried sending the message of (1,0) upon system start, but that does not work.  Is there something special that needs to be done to set up the MC050-020 as a CAN Master?  What else could I be missing?

Offline Jakob

  • PLUS+1 Expert
  • ****
  • Posts: 98
  • Karma: +2/-0
Re: CANopen Master
« Reply #1 on: May 13, 2014, 11:00:01 AM »
Have you tried sending the start command with CAN-king, or is it being sent by the MC50?



NickFro

  • Guest
Re: CANopen Master
« Reply #2 on: May 15, 2014, 05:07:04 PM »
I have tried doing both.  Neither have been successful.

NickFro

  • Guest
Re: CANopen Master
« Reply #3 on: May 15, 2014, 06:56:34 PM »
I figured it out.  It was a simple mistake.  The Baudrate dip switches were backwards, and therefore I had the module set to the wrong Baudrate.