Author Topic: JS6000 & JS7000 CAN Function Block TimeOut Output  (Read 4154 times)

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 191
  • Karma: +36/-1
JS6000 & JS7000 CAN Function Block TimeOut Output
« on: November 30, 2021, 12:37:41 PM »
The CAN receive function blocks for the JS6000 & JS7000 have two signals TimeOutBJM and TimeOutEJM.

The user manual for the CAN function blocks state that these signals indicate if the function block receives the respective messages within a 100ms timeout limit (T = Message not received within 100ms limit, F = Message received within 100ms limit).

I am having an issue with these blocks as both are not indicating the timeout unless they have received at least one message. Is anyone else seeing this?