PLUS+1 Software > Displays
DP700 BusOn
(1/1)
macbahi:
Hi!!
I had BusOff and the red led blinking.
It was done because the can cable was damaged.
I make new cable but the red led stay blinking.
My question is't possible to make BusOn without restart Display.
Thanks
Mac
Tor:
Hello macbahi,
When the controller goes to BusOff it tries to reset itself a number of times (5 times is default).
This number can be set in the Unit_Config block in the application template. You can also add a manual reset signal, in addition to the existing one. Read the API before before doing this.
If you don't have a manual reset signal you need to restart the unit.
Have a nice day.
Navigation
[0] Message Index
Go to full version