PLUS+1 Software > Displays
DM1200T bluetooth
(1/1)
jwestcott23:
Has anybody tried to use or connect to the bluetooth available on the DM1200T? I have the interface enabled, have it set to discoverable, and set autopairing to true just so that i could try to get connected to it. I had it show up on my phone as available only one time and when i tried to pair with it, i got a message on my phone that there is an app needed for pairing ??? ? I was just wondering if anybody had some advice or maybe a sample that would help me.
Thank you!
Tor:
Hi,
I have not played around with the DM1200 and mobilephones enough to help you with this setting. Maybe someone else has a good answer.
Please contact the PLUS+1 Helpdesk and create a case if you still have problem: https://danfoss.secure.force.com/dpscustomersupport
Add to the case what HWD file and what type of phone you are using, as much details you can.
Navigation
[0] Message Index
Go to full version